This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2379 with Powerdesign PD9501G issue

Hi 

I was validating the detection and functionality of the TPS2379EVM(PWR106). I try to power on with 60W Power design POE model number PD9501G.

I observe the PSE port power is blinking. When i check the waveform with oscilloscope i observe the 48V is given by the PSE and again removes the power. Do you have any inputs?

The test is performed with EVM and keeping the J6, J7 not placed. I observe the T2p also not detected.

When i connect the oscilloscope probe after few cycles of that it detects and gives the power(This is some times) but the T2p LED is not turning on.

The above test are performed without any load to the circuit. Even connected load for the VDD, VSS nets and observe similar behavior.

please let me know.

Regards

Nagaraju