Hi,
I find that TPS544C20 have two different ground pin as following describing:
"AGND: Analog ground return for controller IC. AGND should be connected to AGNDSNS
(Pin 13). AGND should not be connected to PGND, GND or the Thermal Tab. All
circuit connections to AGND should return to this pin and not be connected to the
AGND to AGNDSNS connection.
GND: Electrically Connected to Source of Synchronous Rectifier. Connect to PGND,
GND, Input and Output Capacitor Grounds"
As I know ,we usually connect two nets together at an point or with a Fe bead finally.
So I wanna know that Is there any potential risk if I connect those two net together directly?
What's the difference between connectiing and isolated.
Do you have any analyze report about this action?
Thanks.