This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51206 VTTREFTOL

Other Parts Discussed in Thread: TPS51206

Hello

My customer are using TPS51206 for DDR3 at Base Station.                        

I have a question from Customer. I'd really appreciated it if you could support me.

From Datasheet, VTTREFTOL is as below.

|IVTTREF|< 10 mA, 1.2 V ≤ VVDDQSNS < 1.5 V    min48.75%  max51.25%

This mean that  VTTREF is min666.5mV and max683.4mV at VDDQ=1.35V.

My understand is correct ?

If my understand is correct, could you please let me know the actual performance of VTTREF.

I don't need you guarantee.

My customer need actual perfomance of VTTREF when they calculate at worst case/condition.

 Thanks

Best Regards

Koji Hori

Marubun