Hello,
I found a circuit from the document "SLVA663" Low cost, Single Inductor Non-Isolated AC/DC LED Driver Design using TPS92314. This is the only one circuit that no need the transformer that I found.
For this circuit's output is 29V, 230mA, I would like to change the output to
1- 24V, 200mA/ 4.8W
2- 24V, 300mA/ 7.2W
3- 24V, 400mA/ 9.6W
Is this circuit possible to change to these output value? If yes, how?
Also do you have the calculator for this reference design circuit?
Thanks & Best Regards,
Steve