In my test device the TPS2511 has 2 switch settings for 550mA+ and 1000mA current limiting with 82K and 47K resistors respectively. However ive been testing with solar panels and batteries (with a boost converter output at 5V) and for currents less than 1A (tested with range between 150mA and 900mA) the output short-circuit current is anything between 80mA and 150mA only.
A more stable test params were :
input :5V, 850mA
TPS2511 output: 5V, 150mA measured with a 10ohms resistor load
with a 82K current limiting resistor for 500mA+ output current.
Shouldn't it be giving out the full input current at least ? What could be wrong here ?
Regards
Soumitra