This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power Module PTH08T230WAD query



Hi,
 
We are using PTH power modules in our design and there is an issue with the functioning of Power Module PTH08T230WAD.
 
The Power module is designed to generate 1.5 V with 12 V as input. We get 0.9 V when measured with Multi meter. when we measured using CRO, voltage spikes are found between 0.9V and 1.5V. Following are the captured waveform and schematics.
Item Description MFG Part NO Reference
1 IC 6-A, 4.5-V to 14-V INPUT, NON-ISOLATED,
WIDE-OUTPUT, ADJUSTABLE POWER MODULE
PTH08T230WAD U47
2 CAP TANT 330UF 6.3V 20% 2917,ESR=10mOHM T530D337M006ATE010 C388
3 CAP CER 47UF 6.3V 20% X5R 0805 CL21A476MQ9LRNC C1347,C1429
4 RES 6.98K OHM 1/10W 1% 0603 SMD ERJ-3EKF6981V R789
5 RES 56K OHM 1/10W 1% 0402 SMD ERJ-2RKF5602X R796
6 CAP ALUM 330UF 16V 20% SMD PCJ1C331MCL1GS C307
7 CAP CER 22UF 16V 10% X5R 0805 C2012X5R1C226K125AC C1361
Please help me in addressing  this issue.
 
Regards,
Vijetha H.N