Other Parts Discussed in Thread: TPS22965
What happens, if an output of TPS22965 connect to ground ?
Does it burn and smoke?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS22965
What happens, if an output of TPS22965 connect to ground ?
Does it burn and smoke?
Hi Hirotsugu,
The TPS22965 does not have internal current limiting, so if the output is connected to ground while the switch is on this could cause excessive current through the switch. If the maximum current ratings of the device are exceeded this could reduce lifetime and cause failures.
When the switch is turned off, there is an internal quick discharge path from the output to ground. So in this case, the device would be protected if the output were connected to ground.
Regards,
Adam Hoover
Applications Support Engineer