This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24055

This is regarding BQ24055 IC:

The battery is fully charged, the charge current drops below the termination current, the CHG LED is off and the CHG pin goes to high impedance; however I am measuring 0.511V on the TS pin. Why is the TS pin not out of its normal charging range? 

  • As long as power is applied, the TS pin is sourcing current into the thermistor.  0.511V is in between the V(TS-10)=790mV and V(TS-45) = 278mV voltage thresholds, meaning the battery temperature is between 10C and 45C.