Hi Team,
I am trying to minimize queiscent current as much as possible in an application where a TPS61221 and TPS61222 are used to boost a single cell NiMH battery (1.5-V) up to 3.3-V. The 3.3-V rail will then be boosted to 5-V. This is a battery powered application so queiscent current is the chief concern here because of a low duty cycle.
Do the surrounding biasing components, specifically C1, C2 and L1 in the simplified schematic in the data sheet, effect Iq significantly? The load will be using very low current, should L1 be selected to reduce or increase the switching frequency to optimize this application?