I know this has been asked before but there has yet to be a response.
We were looking to use the BQ51003 in place of the BQ51013A in our design because it is characterized for the lower power of our system (~80mA). However, the behavior of the two differs in the packet sent out when the TS/CTRL pin is pulled high: (Packets monitored with Avid Tech Qi Sniffer v1.1)
The BQ51013A-EVM sends EPT - Charge Complete and the transmitter responds by setting LEDs to indicate this state. After a brief time a new power transfer cycle is attempted.
The BQ51003-EVM sends EPT - Unknown and the transmitter responds by setting the LEDs to fault mode. The transmitter waits for the receiver to be removed and replaced before attempting a new power cycle.
Why is there a difference? How do we send the Charge Complete packet?
The behavior is the same if the EN1 pin is pulled high rather than the TS/CTRL pin.
If we can't use the BQ51003, how do we return the two evaluation kits we ordered?