Hello,
I have an old design that uses eight LM317T regulators to regulate DC voltages to eight separate audio channels. This old design is from the early 1990's and the board layout was done with velum and tape. We are now seeing the LM317's oscillate in some of the production units. We have not seen this in the earlier builds. What has changed in the LM317 in the past 15 years or so? Has the error correction amplifier gotten faster? Has the gain bandwidth of any of the internal components improves? The oscillations that I am seeing are 10 to 20 MHz and because of the poor layout, the noise is easily coupled from one channel to another. Thank you for your help.
Rich