Dear Sir,
Need your help to suggest a suitable LED driver with following specs:-
Input voltage range : 3V to 9VDC
Output : 3.4V at 1 Amps (single WLED)
or
Output : 3.4V at 700mA (single WLED)
This calls for a buck-boost converter. Which is best suited device - TPS43000 ? ? ?
I also need the schematic with component values with the device that you suggest
The customer wants to use this scheme for Single LED Table lamp / Reading lamp.
The annual volumes are approx 12K in first year
The expected MP date is May 2010