This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950

Other Parts Discussed in Thread: UCC28950

The tolerance of resistor 825kΩhookuing up ss pin as outside

synchronous behavior.

 

When synchronous signal input SYNC pin from outside, the datesheet is written to connect resistor at 825kΩ

In parallel, but How  many acceptable range is this resistor ?

 

Presently, I architect part of additional voltage slope of UCC28950, and I would like to question about

TI SLUA560B "UCC28950 600-W Phase-Shifted, Full-Bridge Application Report.

 

Variation calculation formula of trance excitation current of

formula 144

 

I calculate ΔILmag by off duty(1-Dtyp), but if I think how to apply voltage to trance, I think on duty how to calucurate. 

Why is off duty?

 

Vslope2 calculating formula of formula 46

I understand this division by trance winding fraction a1 to convert current amount of change dILout to 1dimension, but it divide 2 in addition.

What is this reason?