In reference to the user guide of the bq25504EVM, I am quite confused about the EVM operation.
For cold start operation, at least 0.4 V, 170 microAmp, or 50 microWatts input power is required under no load condition. If I want to connect a 3 V battery at the BAT pin and charge with using a dc supply with the above input power, how will the battery get charged under no load condition?
I am confused about about the working relationship between the Vstor and Vbatt junctions.
How does the Vstor come into play? Does the battery charging operation depend on what voltage the battery is currently at?
Any help will be greatly appreciated.