Hi,
I have some question regarding the TPS62122EVM, the eval board for the
TPS62122.
1) On page 3 of the EVM datasheet it says that certain pins such as vout (J4) and ground (J3) need to be twisted and kept as short a possible. What exactly does that mean?
2) If I connect a wire between EN ON and JP1 that will allow the board to be turned on while connecting the wire from EN to off will disable the circuit from being used correct?
3) If the circuit is forced to be off and a voltage is given to VIN does damage to the component occur.
4) Is there any way to change the output voltage of the device besides having to solder in new resistors, and if it has to do with the forward feed capacitor can you explain what its purpose is?
5) Do I need to correctly configure J7 in order for the device to work properly or do I only need a component soldered in the J7 pins if I want to measure to noise spectrum?
Thank You