Hi,
I am trying to synchronize a UC3886 and a UCC38C40 using the technique introduced in the UNITRODE APP NOTE U-111, injecting SYNC pulse signal through a 24 ohm resistor connecting between CT and ground. The problem is that the output PWM is not stable in the open loop performance. Here is how I set up the circuit.
The UC3886 is programmed running at 100KHz and a 1.9V voltage source is connected to the pin 1 CAO/ENBL to output a 50% PWM. The circuit was running as it was designed. After this, a 24 ohm resistor is put between CT and ground. A 110KHz ,10% duty cycle and 1V peak pulse signal is injected at the connection of 24 ohm and CT. The output PWM was not stable at all, the duty ratio varied cycle by cycle in big range(about 20%).
What should I do with this technique?
He,Siyu