This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Query reg BQ34Z100

Hi TI,

As per data sheet it is mentioned "Upon detecting A/D value representing 2.5 V on VEN pin, Four-LED mode will display the RSOC by driving pins RC2(LED1), RC0(LED2), RA1(LED3),RA2(LED4) in a proportional manner where each LED represents 25% of the remaining state of charge. For example, if RSOC = 67%, three LEDs will be illuminated."

Should it be 75% instead of 67% if three LEDs are ON ?

Also please confirm the below:

One LED ON: 25% ROSC

Two LEDs ON: 50% ROSC

Three LEDs ON: 75% ROSC

Four LEDs ON: 100% ROSC (Full Battery Condition)

Please reply ASAP.

Regards,

Deepak Holla.

  • Deepak,

    I would expect only two LEDs to be lit for a 67% SOC. They may have been thinking about a five LED setup when making that statement.

    Tom

  • Hi Tom,

    I am afraid my question is still not answered.

    Consider the case of using the direct 4 LED case.

    Please confirm if the below is correct:

    One LED ON: 25% ROSC

    Two LEDs ON: 50% ROSC

    Three LEDs ON: 75% ROSC

    Four LEDs ON: 100% ROSC (Full Battery Condition)

    If not then please provide the percentage of remaining state of charge indicated by each LED in 4 LED case.

     

    Regards,

    Deepak.