This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65217C with supercap instead of battery - for graceful shutdown of AM335x

Hi, wanted to ask officially - is it possible to replace battery with supercapacitor - in  TPS65217C ?

I cannot use batery ( due to device liftime requirements), but 5V 4F battery would provide me with enough energy to shutdown and store all data ( I use barebone mode with SPI/MMC storage )

Some threads suggest it should be pretty simple:

http://e2e.ti.com/support/interface/industrial_interface/f/142/t/206970.aspx

> A TI employee said [1] "The battery charger should work fine with a 
> supercap.  You'll need to make sure the TS (battery temp sense) pin 
> is at a proper voltage to allow charging.  If the supercap does not 
> have a temperature sensor, you can simply put a 10k resistor from TS 
> to GND." 

Then just configure pmic to charge to max voltage ( 4.25V ).

Well, I might also have to tweak voltage sense to allow charging empty capacitor. Maybe add side resistor/diode circuit to charge it to e.g. 2V - so it is recognizable as connected ?

One more question - how long will the PGOOD stay good when operating with battery - as you cannot easilly maintain 3.3V on LDO? Does it cut off at 3.3V level ? ( I am asking as documentation says that the chip works with battery from 2.7V )

 Or maybe ( as I use Vac only) - connect supercap on Vusb ( with separate charging) ?