This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps65261 start up, on VDIV

Other Parts Discussed in Thread: TPS65261, TPS3808

My customer TQS would like to use use the internal VDIV of the TPS65261 instead of the TPS3808 supervisor.

He would like to detect 4.6V vin as minimum then generate a flag to the MCU.

 Now the questions are :

How accurate is the threshold of 1.23V on VDIV

What happen at reset pin when the input voltage VIN is less than 4.5V? or at startup phase? Or at transient input voltage 5V  to 3V then back to 5V