Hi,
I'm a bit stuck with the selection of the right step down converter and a fuse circuitry. The step down converter has an input voltage of 12V and an output voltage of 3.3V. Of course, it is a good idea to fuse the input side of the converter in case it is damaged. But is it necessary to adjust the fuse size such that it blows when the output side of the converter is shortened?
For example, the TPS62132 has a short circuit protection where it limits the current to 1.6A whereas the maximum output current is 3A. Is it necessary to fit the fuse size on the input side of the converter to the output 1.6A? Or can I just leave the converter enabled even in case of a short on the output side?
Thanks!