Hello,
I have two questions about BQ24133.
1.
Fast charge current is 1295mA(typ).
Rsr is 10mΩ.
Charge termination current is 130mA(typ).
Is charge termination current(min) 130mA * 0.6 = 78mA? (Vsrp-srn=2mV)
Or is it 120mA?
I read page-8 of the datasheet.
Note-3 "The minimum current is 120 mA on 10mΩ sense resistor."
2.
Because fast charge current is small(1295mA), is it better that I use a larger Rsr(e.g., 20m Ω)?
This purpose is to raise the precision of the charge termination current.
Regards,
Daisuke