Customer has a TLV431 part with the part marking "YAIL". Can you tell me if the part markings is for TI voltage ref part TLV431CDBVR or TLV431AIDBVR? Both of these two parts are listed on the AVL so the customer doesn't know which one they have.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Customer has a TLV431 part with the part marking "YAIL". Can you tell me if the part markings is for TI voltage ref part TLV431CDBVR or TLV431AIDBVR? Both of these two parts are listed on the AVL so the customer doesn't know which one they have.
Tom,
YAII is TLV431AIDBV
Y3C_ is TLV431CDBV (_ is one of three chars; 5, 6, I)
There are no devices with YAIL as a marking.
http://www.ti.com/general/docs/partmarking/partmarkinglookup.tsp
Hi Tom,
If you go to the PART MARKING page, http://www.ti.com/general/docs/partmarking/partmarkinglookup.tsp?startPosition=0&navigationId=0&templateId=0&siteFlag=0&keyword=YAIL&searchType=device&TICOM_AUTHLEVEL=3&TICOM_VALIDATE_INPUT=1
enter the part numbers, you'll get this information:
| Device Name | TLV431CDBVR | |
| Description | Low-Voltage Adjustable Precision Shunt Regulator | |
| Pin / Package | 5 / DBV | |
| Status | ACTIVE | |
| Device Mark |
|
| Device Name | TLV431AIDBVR | |
| Description | Low Voltage Adjustable Precision Shunt Regulator | |
| Pin / Package | 5 / DBV | |
| Status | ACTIVE | |
| Device Mark |
|
YAIL is not listed, so perhaps the last charcater is not read correctly, could it be an "I"? In fact, if you enter YAIL, no device is returned; YAII shows the TLV431 device.
~Leonard