Hello everybody.
I am making a synchronous buck converter of 200kHz. It’s in open loop right now. A schematic diagram is presented in Fig. 2 and description of circuit elements are detailed on table 1.
Fig. 2. Synchronous buck converter.
Table 1. Elementos del circuito de la figura 2.
Elemento |
Referencia |
D |
STTH8ST06 |
Q1, Q2 |
STFI40N60M2 |
Driver |
UCC27201D |
Cin |
10uF/50V |
R1, R2 |
10KΩ-1/2W |
L |
74435584700 WurthElectronics |
C |
330uF/100V |
Rs |
0,05Ω/5W |
Figure 3 is a half bridge drive to switch Q1 and Q2 MOSFETs. UCC27201 is a 8 pin SOIC package of TI. The implemented circuit has a boostrap capacitor (CB) of 470nF and every MOSFET has a 6.8 Ω resistor in series with gate pins.
Fig. 3. Half bridge driver.
Fig. 4. PWM Q1 signal measured from microcontroller pins.
Fig. 5. PWM Q2 signal measured from microcontroller pins.
Figure 4 and figure 5 are PWM signals for Q1 and Q2 MOFETs, respectively, measured from microcontroller pins without power stage (inductor, capacitor and low). PWM signal has a dead time of 250ns (about 5% of dutycycle).
Fig. 6. Vgs of Q2 measured from MOSFET without power stage.
Fig. 7. Vgs of Q2 measured from MOSFET with power stage.
Fig. 8. Top: Vgs Q1, Bottom: Vgs Q2, measured from MOSFETs pins with 30V powered converter and a load of 1.14 A
Converter has a 17.2V with a dutycycle of 56% but according to figure 6, PWM signals have high frequency oscillations and when Q1 is turning off and Q2 is turning on, there is a short time when both MOSFETs are ON at the same time (I couldn’t solve this problem even put a dead time of 1us which is about 20% of switching period).
Given that increase the timeout is not enough, How to improve the driving state transition from Q1 to Q2?
Fig. 7. Drain-source voltage.