This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Isolated DC-DC converter to supply the TPS65381-Q1

I have a DC voltage in the range 9-15 Volts available to supply the multi-rail power supply TPS65381-Q1, which is fine, but unfortunately I need galvanic isolation, i.e. an isolated DC-DC converter with a transformer. Any suggestions for a suitable device/application will be appreciated. It should be capable of supplying current corresponding to the current limit (1.4A) of the pre-regulator of the TPS65381-Q1.