Hi Team,
I have an application where I want to charge a very high capacity battery (~10-15Ah) from a ~20-V/1.5-W PV cell.
I was looking at bq24210 but noticed a forum thread saying the pre-charge safety timer might be an issue with a low charge rate on large batteries.
How would the pre-charge safety timer cause an issue with large battery packs? Is there a device that I can use instead of the bq24210?
Also, would a bq24210 charge any lithium chemistry pack? Example: LiSOCl or LiSO2
The charger would also need to be qualified for a -40 to 85 C range.
Regards,