This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
You might want to cross-post in the LED driver forum. They may have a solution.
I don't personally support, or have any specific knowledge of TPS61020. Let's see if someone from that product line will respond.
Hi Yaita,
This application can be used in LED driver.
As you mentioned, when adding a PWM signal at the "flash lighting control", it only turns on/off the LED. When it turns on, the current is fixed. So this solution can not change the current directly. However, if the PWM signal changes its duty cycle and have enough frequency (for example higher than 100Hz), it can change the turn on time of LED, so that the brightness can be changed, which is equivalent to changing its current.
BR
Gene
Hi Yaita,
1) You're correct, this method can not regulate the current precisely.
2) Remove the resistor R1 and R2, add a resistor in series with Q1 to ground and then connect the FB pin so that the current can be controlled precisely. Just be careful of the resistor power consumption and value variation with temperature.
BR
Gene
Hi Yaita,
Please connect the FB pin to the point between Q1 and R1 and remove C3. Besides, please connect both EN pin and Gate signal of Q1 to PWM dimming signal. In this way, when Q1 turns off, it won't regulate the output voltage.
BR
Gene