Hi,
I am facing issue with BQ24190 Battery charger. I am setting the following register values & getting REG08 content as charger port is detected (USB host/ Adapter Port) but it is not charging. And fault register values is 0x00 only.
Even sometimes it is showing the battery is charging, but at that time the current is not entering to battery.And the charger also not getting detected.
What will be the issue? can you please help us,
REG NAME | DESCRIPTION | REG VALUE | REG VALUE | NOTES | ||
REG00 | Input votlage limit - 5V and Input Current limit 1.5A | 0X75 | 0X75 | 0x05 | ||
REG01 | Charge Battery, System Voltage limit - 3.7V, | 0X1F | 0X1F | 0x11 | ||
REG02 | Charge Currnent - 2A | 0X60 | 0X60 | 0x60 | ||
REG03 | Precharge - 256mA; Charge termination - 128mA | 0X10 | 0X10 | 0x10 | ||
REG04 | Charge Voltage Limit: 4.192 | 0XAE | 0XAE | 0xb0 | ||
REG05 | Watch dog timer disabled | 0X8A | 0X0A | 0x0a | ||
REG06 | Default | 0X03 | 0X03 | 0x03 | ||
REG07 | Default | 0X4B | 0X4B | 0x4b or 0xcb | ||
REG08 | 2d | 2d | 0x44/0x84 | REGISTER VALUES AFTER SETTING REG[0:7] | ||
REG09 | 0 | 0 | 0x00 | |||
REG0A | 23 | 23 | 0x23 |
Waiting for your faster reply,
With thanks,
Ganesh.