This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power Supply Topology for AC powered Device?

Other Parts Discussed in Thread: UCC28700, TPS62230

Hi, I'm working on a design for a new device.

It needs to be powered from an AC ( 100-265VAC ) power source.    I need an isolated 5VDC at about 500mA, as well as a non isolated supply at 3.3V at about 150mA

The isolated 5V supply is for running a microprocessor plus some associated driver circuits.

The non isolated ( with respect to the AC ) 3.3V is for powering an IC and opto-isolators, the IC is sampling data from the AC power supply.

I'm considering using a UCC28700 controller to provide the isolated side,     I'm debating how to do the 3.3V side and would appreciate any comments.

Options;

(a) use a cpacaitve power supply for the non isolated side. Quite simple but the capacitor gets pretty big and chunky.   I'd need something thats 1" x 1" x .75" and those parts are not so cheap.

(b) have a second AC/DC non isolated converter, just for the 3.3V.

(c) Use a DC/DC isolated converter to convert the "isolated" 5V to a 3.3V on the non isolated side.   This right now looks like my preferred option.

Any comments?