Hi, I am building some modular boards for prototyping. I have designed a USB based solution for 3.3V using a BQ24392 negotiating high current for a TPS62086. Now I would like to add a compatible optional battery module that is a complete Qi receiver, battery, and charger 'in a box'. I can provide the 5V line from the USB as well as negotiation signals from the BQ24932 and obviously the 3.3V for the system. I know there are dual input chargers and that combined with a BQ51013B would work for all but OTG output. What I am wondering though, would I need a simple buckup for the OTG then? Is there any safe/cheaper way to utilize something like a BQ24295 and some isolation logic to allow for charging by Qi if present, otherwise USB charging or OTG supply? Is it better to utilize a BQ51050 for Qi and have two chargers?