This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53355 / maximum output capacitance, load transient data

Guru 20090 points
Other Parts Discussed in Thread: TPS53355, LMZ31530
Hello,
 
Please let me know the following.
 
1.  Cout (max)
Could you please let me know the maximum output capacitance value of TPS53355?
If there is no specification, please let me know the tested data of maximum Cout ?
Since this is Dcap mode , ‎we can use any Cout value if we add the ripple injection.
However LMZ31530 has specification of Cout(max).
2. Load Tansient data
Could you please let me know the load transient data of the following conditions?

Vin:12V
Vout:1.5V
Iout:300mA -->30A within 100ns, 30A ---> 300mA within 100ns (i.e, about  di/dt=0.3A/ns)
I can find the load transient data from datasheet.
However, di/dt is 2.5A/us.
Please share the data if there are similar conditions data.

Best Regards,
Ryuji Asaka