This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78PL116 current draw after charging done

Other Parts Discussed in Thread: BQ78PL116

Hi.

I have this next issue with the circuit i have developed with gas gauge bq78pl116 and I need some help, as I am not sure what I am doing wrong.

So this happens:

1. I am doing a charging cycle.

2.COV or POV is reached

3.Charging mosfet stops the input 

so far so good but... while the pack it`s resting I see that there is a current leackage over the sense resistor of about 250mA

what is causing this?

when resting is done and I can draw or charge the pack the current is back to 0-50mA.

what am I doing wrong? 

I must specify that I do not use the pump or balancing right now.

I am trying to make the aux file.

Thank you very much for your time for reading / replying to this issue.