Please let me about SS/EN pin connection of TPS54610.
If SS/EN pin connect 5V pull-up, is it normal operation?
Or, is it have any problem?
Best regards,
Satoshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SS/ENA is internally pulled up. It is intended to have a SS capacitor connected between SS/ENA and GND to control the output voltage slew rate at start up. You can actively hold the SS/ENA pin low, to disable, then release it to allow the normal start up sequence. The abs max voltage on SS/ENA is 7 V, so it will not be damaged directly, but I do not think I would recommend tying SS/ENA to a higher voltage than VIN. In any case, it should not be necessary to pull SS/ENA high externally.