This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq78pl116 .aux file generation problems

Hi there guys.

It`s me again, this time is because I get some errors on generating of the .aux file.

So I did the 15th steps in the slua505b, and I have a csv file with the logs needed to generate file.

although all was ok, with the logging and so on, I still have a problem generating aux file.

The parameters I set are as fallows : 

6 cell in series

parallel cels is 1

1st discharge current is 5330mA

pack capacity is 11000mA

I am not sure why the logging of the capacity is 5330/10, I am using the 10 times option, but not sure why i am logging current/10.

anyway, I am attaching the file and maybe you can help me.

the chem id is 1148

And please tell me what I was doing wrong.

the csv file is the one generated, no modifications or so.

thank you very much 

aux file day 2.zip