We have a battery pack running with the BQ78PL114, new firmware (5k).
The cell voltage is limited to 4.1V.
The chemistry data is selected to ID 204 and the cell is the Sanyo 18650W.
I load the .aux file generated out of the logged data. During data logging, 4.1V has been End Of Charge Voltage.
Approx. only 84 % RSOC is displayed, if the cell is charged to 4.1V. If the cell is charged to 4.2V, 100% is displayed.
Do i need an other chemistry data file for the end voltage of 4.1V, or should the generated .aux file be enough?
Regards
Andreas