Hello I am planning on using the LM3481 as the primary side controller for a 25W flyback converter. Is it possible to use a TL431 and Optocoupler to implement the feedback? Because this feedback method already does compensation I noticed that in this design by TI the feedback pin is grounded and the optocoupled return line is connected directly to the compensation pin, bypassing the error amplifier. (picture attached).
Perhaps you could recommend a more suitable low cost, low component primary side controller. I was also looking at the UC3843
Thanks!
Erik