Dear all.
Do you have maximu value of theta ja of TO-252?
Regards,
PAN-M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all.
Do you have maximu value of theta ja of TO-252?
Regards,
PAN-M
LM317AMDT (TO-252) Thermal
No of Pins : 3
Package Designator : NDP
Die Size :1676.4 X 2286 um
Theta JA-High K : 51.0°C/W (PCB per JESD51-7)
Theta JC, top : 64.1°C/W
Theta JB : 28.6°C/W
Psi JT : 21.2°C/W
Psi JB : 29.1°C/W
Theta JC, bottom : 0.9°C/W