Hello,
How should the resistance of Iset calculate?
Must I use 25mohm for Rsense?
Best Regards,
Kei
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
How should the resistance of Iset calculate?
Must I use 25mohm for Rsense?
Best Regards,
Kei
Hello Kei,
Kei Sato73562 said:How should the resistance of Iset calculate?
Formula is on page 26 DS.
Basically for 150mA/ch scale and DISP_CL1_CURRENT=0xFFF (max current) formula can be simplified: ILED= (24/RISET)*150, where RISET kOhms. ILED mA
Kei Sato73562 said:Must I use 25mohm for Rsense?
Not necessary, but you have to be aware BOOST_IMAX_SEL current will be scaled.
During design time all parameter were simulated with 25 mOhms.
Best regards,
Vladimir