Hello Dears:
I bought a Zedboard (with Zynq). This board utilized 3 pcs of UCD9248.
i need help, I want to know how i can adjust the voltage on the rails of this pcs using the command of PMbus.
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Fusion Digital Designer can create a text file with the necessary PMBus commands.
I wonder whether xilinx or the Zedboard vendor can provide you with the default configuration for the UCD's.
A xilinx web page mentions a linux driver to access the UCD9248:
https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/Documentation/hwmon/ucd9200
Do you want to do the access to the UCD's while running Linux do you run your own software?
Andreas
hello,
thanks for your answer
i want to access to the UCD's while running Linux, that all for the exploration about power consumption of the system.
Mohamad
Yes, it is possible to adjust the output voltage of a rail controlled by the UCD9248 with PMBus commands, as long as the board provides access to the PMBus interface and they have not used the security command to block VOUT_COMMAND.
Unfortunately, our PMBus tools do not support Linux, you will need to provide your own method to output PMBus commands to the controller.
Here is the link to the UCD92xx PMBus command reference, it lists supported commands and details for manufacturer's specific commands:
www.ti.com/lit/ug/sluu337/sluu337.pdf
For details on standard commands, refer to the released PMBus Specification at www.pmbus.org , the UCD9248 supports version 1.1 of the PMBus Specification