Hi All,
is it necessory to give bias voltage to TPS74012 when we are using it in fixed operation mode. what happens if we did not give a voltage to bias pin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
is it necessory to give bias voltage to TPS74012 when we are using it in fixed operation mode. what happens if we did not give a voltage to bias pin
Hi Dinesh,
A bias voltage is required for this device.
The bias voltage is used on high current devices to allow for a really low dropout specification, reducing the power dissipation across the LDO.
An example of this with the TPS74012:
If Vin=Vbias, Vin(min) = 1.2V+1.6V = 2.8V. Pdiss = 1.6V*1.5A = 2.4W are dissipated across the device.
But if Vbias = 3.3V, Vin(min) = 1.2V+0.3V = 1.5V. Pdiss = 0.3V*1.5A = 0.45W are dissipated across the LDO, nearly a 2W reduction in power dissipation.
Regards,
David