This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62730 higher output currents

Other Parts Discussed in Thread: TPS62730, TPS62740

For a WSN application I need a DC/DC converter with 2.1V fixed output and bypass mode. Sadly, the only available DC/DC converter of these characteristics is the TPS62730 that supports a maximum output current of 100mA.


I have current peaks of around 175mA during about 10ms and I need the output voltage not to turn down. I thought of using a big capacitor on the DC/DC output to maintain the output voltage during these current peaks, what do you think?

Another idea I had was using two TPS62730 in parallel, but i'm not sure about the consequences.

Thank you very much in advance.