HELLO I NEED TO NO TO GET ALL THAT I WOULD NEED TO GET STARTED WITH THE ABOVE DEVICE I NEED TO NO WHAT DO I NEED TO DOWNLOAD
I HAVE THE FUSION DESIGNER SOFTWARE
AND THE FUSION GUI SOFTWARE BUT I CANT OPEN IT
WHAT SHOULD I DO
NOW I NEED TO MAKE A DEMO BOARD TO PLUG UP TO THE PC TO PROGRAM THE PART AND A LIST OF SAMPLE CIRCUIT TO PLAY AROUND WITH TO SEE HOW THE DEVICE REACTS TO THE CHANGES MADE
IT WOULD BE A BIG HELP IF SOMEONE CAN CALL ME DIRECT SO I CAN ASK QUESTIONS ANS LET YOU NO WHAT IAM TRYING TO DO ,I NEED TO COMEUP WITH A PART THAT I CAN USE IN PHASE MODULATED PWM APPLICATION TO DRIVE A FULL BEIDGE AND THE OUTPUT TRANSFORMER WILL GO ACROSS THE HALF BRIDGE LEGS AND THE SEC. SIDE OF THE TRANSFORMER WILL PRODUCE 175VAC PK-PK AND THE HIGH VIOLTAGE SQ. WAVE WILL GO ACROSS A LOW PASS FILTER TO GET THE SINE WAVE OUT OF APPROX 125VAC RMS OPEN LOOP AND CREATE A FEEDBACK NETWORK / DIVIDER TO FEED BACK TO THE PART TO CLOSE THE LOOP AND REGULATE IT DOWN TO 115.00 VAC AT 400 HZ
THIS WILL BE A PHASE SHIFTED PWM CONTROLLER AT 115 VAC FROM FULL LOAD TO NO LOAD AND OUTPUT STAYS CONSTANT, AND HAD HAVE OVP ,UVP OCP OVER TEMP CONTROL AS WELL
WHAT ALL DO I NEED TO GET THIS GOING ,
FIRST I WILL TAKE THE P/N U3138064CD AND MAKE A DEMO BOARD ARE A DAUGHTER BOARD THAT WILL GO OVER THE MAIN DRIVER BOARD ARE CONTROLLER FOR THE SYSTEM SO THAT ONCE THE UNIT ARE MADE I WILL PLUG THEM UP TO THE PC TO PROGRAM THE BOARDS AS REQUIRED
SO LET ME NO PLEASE THIS PROJECT WILL HAVE A 100000 PC FIRST RUN THE RUNS ARE IN 4 SECTION
SO THE QTY WILL CHANGE PER APPLICATION SO LET ME NO PLEASE ASAP WHAT I NEED TO GET THE ADAPTER BOARD READY FOR THE CONTROLLER TO BE PROGRAMMED