This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM34926 VIN=100V operation



Hi 

Our customer are interested in LM34296.However there are some concerns.

- Is this device assumed the operation in VIN=100V even if it's instantaneous?

    The absolute maximum voltage at VIN is 100V. The voltage of BST pin will exceed 100V when it operate VIN=100V.

     However there is no definition BST to  GND. 

- In relation with above question, does the internal MOSFET has the absolute maximum voltage same as VIN?

The customer's application is telecom. They are concerned about the situation, such as around VIN=100V

Regards,

Koji Hamamoto