This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS75933 Oscillating

I am getting oscillations when using the TPS75933.  I have tried an assortment of input and output capacitors, some of which change the frequency and power level of the oscillation, but none of which cured it.  Does anyone have any ideas as to what could be wrong?  This is a 7.5A part and I am drawing approx. 4A.  I believe I am operating in the stable region, but something must be wrong.  Below is a pic of my schematic, it's very simple.  Any help would be greatly appreciated.


Thanks,

John