This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61170EVM demo board



I am trying to change the output voltage of the demo board by applying a 50kHz PWM signal to the CRTL pin. However the output voltage is not stable. Under load conditions (150mA) I can only change it from on and off.

When I use the USB interface I am able to control the voltage as long as there is no load. When I apply the load I see an ACK error and the voltage will not change.