This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2623A Efficiency



Hi,

I'm designing a setup-up converter based LM2623A. It should to converts 3.7V to 5V and minimum 1.4 A, will be very good if provide 1.8A. I have designed the PCB as also assembled it. However the efficiency is very low, and far away from the data sheet. It is around of 58%, when drawing 1A, at 5V output and supply of 4.0V .Drawing higher current is not possible, because the output voltage drop down to 4.2 V on the output. It is also not possible to decrease the supply voltage below 3.8V, because it also results low voltage on the output.

Attached below link to schematic.

https://app.box.com/s/ed3ph9ffkew6d6c82uew

Any advice about my design would be very welcome.

Thank you in Advance

Grazyna