Team,
TPS40170 convert 35V to 24V at 100kHz and 47uH choke with a 1uF SS cap.
While we test a short circuit at output, the TPS40170 is not able to recovery while removing the short circuit.
But if we remove the output capacitance 3000uF, the circuit can recovery from the short circuit.
Or no removing the Cout, but reduce the full load current from 7A to 1A, the circuit can also recovery.
May I know if there is any limitation to cause this happen?
Thank you.