Hey all,
When my customer tries to turn on their WiFi chip through the TPS78233, there are a couple issues.
1, it creates a lot of noise; and 2, it results in much less of a range for the WiFi chip.
When they replace our part with the Maxim part # MAX8891EXK33 it works just fine.
Any thoughts on why this is?
Here are some additional details:
There is a 4.1mA draw without the WiFi chip being on. Once on, it rises to 10mA, with 14mA on receive and 18mA on transmit.
Their products are already in the field, so time is of the essence. I have the gerbers as well if needed (directed towards TI folks).
Thanks,
Kayiita