I am seeing strange behavior during the soft-start sequence. With the output being fed back into VCCX, I am seeing the buck switch completely stop switching (as seen by monitoring the behavior of the SW1 node) for a few milliseconds after the approximate moment when VCCX takes over for the VCC node (i.e., the VCC pin drops from 7V down to ~3.9V).
At this point, the output decays while the buck switch is not switching, but this is evidently NOT the result of a VCC UVLO or overcurrent condition or something of that nature because the SS pin capacitor continues to charge (until FB decays to 150mV below it, at which point SS starts decaying to follow FB) instead of rapidly discharging.
The buck switch appears to start switching again (and SS ramps up again) shortly after the output (and VCCX) have decayed enough such that the VCC regulator re-activates and has brought VCC back up to 7V. It should be noted that as the VCC pin is rising from the internal regulator reactivating, the SW1 node seems some erratic activity as if the buck switch is trying to re-engage. At this point, a slight dip in the VCC pin voltage occurs, but the SW1 activity ceases, and VCC is allowed to finish its rise to 7V.
Any insight into what might be causing this behavior and/or how to avoid it while still utilizing the VCCX pin being driven by the output would be greatly appreciated. Could the values of Cbs and Cvcc have anything to do with this?
Thanks