Hello,
I am using the reference design of the BQ25504 to charge a battery from a solar cell and am able to power the load when it is connected directly to the VSTOR pin.
The problem is that when I attach an external load switch (BAT_OK drives an NMOS which drives an PMOS) to protect the battery from deep discharging, as proposed in the datasheet, I get no voltage at the output.
Any suggestions on the circuit or the type of the FETs I have to use?