This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The absolute-maximum-rating value of BQ20Z45

Other Parts Discussed in Thread: BQ20Z45-R1

Dear, All

About the absolute-maximum-rating value of BQ20Z45-R1, the following is indicated to the datasheet.
- Operating free-air temperature range -40℃ to 85℃
- Functional temperature -40℃ to 100℃
Please let me know the meaning of 'Functional temperature'.

Thanks, Masami M

.

  • We guarantee operational temperature: Ta= -40 to +85,

    i.e.the electrical characteristic tabless are gauranteed over the operational range.

    The wider functional temperature range relates more to the absolute max junction temperature beyond which you will damage the part. Operating at the functional temp should not damage the part but it shouldn’t be running at these extremities since abs max may cause reliability issues with the device.

    These higher functional temps are to allow a customer to run some characterization of their system but we’re not recommending that they use these as normal operation and we are not gauranteeing our electrical specs.

  • Hi, Mike

    Thank you for your reply.
    I answer it to a customer.

    Thanks, Masami M.